Write/Read
About Noise Figure

NoiseAverageFactor Property


Description

Sets and reads the averaging of the noise receiver.

 VB Syntax

noise.NoiseAverageFactor = value

Variable

(Type) - Description

noise

A NoiseFigure (object)

value

(long integer) - Averaging value. Choose a number between 1 and 99.

Return Type

Long Integer

Default

1

Examples

noise.NoiseAverageFactor = 10 'Write

AvgNoise = noise.NoiseAverageFactor 'Read

C++ Syntax

HRESULT get_NoiseAverageFactor(long* pVal)

HRESULT put_NoiseAverageFactor(long newVal)

Interface

INoiseFigure