Write/Read |
About Noise Figure |
Description |
Sets and returns the receiver to use for noise measurements. |
VB Syntax |
noise.NoiseReceiver = value |
Variable |
(Type) - Description |
|
noise |
A NoiseFigure (object) |
|
value |
(Enum as NANoiseReceiverMode) Noise receiver. Choose from: 0 - naStandardReceiver The standard PNA receiver. (Opt 028 or 029) 1 - naNoiseReceiver The noise receiver. (Opt 029 ONLY) |
Return Type |
Enum |
Default |
1 - naNoiseReceiver |
Examples |
noise.NoiseReceiver = naNoiseReceiver 'Write |
|
NoiseRec = noise.NoiseReceiver 'Read |
|
C++ Syntax |
HRESULT get_NoiseReceiver(tagNoiseReceiverMode *pVal); HRESULT put_NoiseReceiver(tagNoiseReceiverMode newVal); |
Interface |
INoiseFigure5 |
Last Modified:
|
11-Jul-2011 |
Edit options |
|
2-Mar-2010 |
MX New topic |