Read-only
About Dynamic Uncertainty

Number Property


Description

Returns the VNA port number.

 VB Syntax

value = port.Number

Variable

(Type) - Description

port

A Port (object)

value

(Long Integer) - Variable to store the returned Port number.

Return Type

Long

Default

Not Applicable

Examples

value = port.Number 'Read the value

C++ Syntax

HRESULT get_Number([out,retval] long *port);

Interface

IPort