Write/Read
About Spectrum Analyzer Markers

OccupiedBandSpan Property


Description

Returns the occupied bandwidth span.

 VB Syntax

value = mkr.OccupiedBandSpan

Variable

(Type) - Description

value

Variable to store the span value.

mkr

A Marker (object)

Return Type

Double

Default

Not Applicable

Examples

value = mkr.OccupiedBandSpan 'Read

C++ Syntax

HRESULT get_OccupiedBandSpan(double* pVal)

Interface

IMarker7