Read-only
About PNOP / PSAT Marker Search

PMaxIn Property


Description

Returns the PMaxIn result of a PNOP and PSAT marker search.

PMax In =  Marker 3 X-axis value

 VB Syntax

pMaxIn = pMark.PMaxIn

Variable

(Type) - Description

pMaxIn

(double) - Variable to store returned value

pMark

A PNOP (object) or PSaturation (object)

Return Type

Double

Default

Not applicable

Examples

pMaxIn = pMark.PMaxIn 'Read

See example program

C++ Syntax

HRESULT get_PMaxIn(double* pNewVal)

Interface

IPNOP or IPSAT