Read-only
About PNOP / PSAT Marker Search

PMaxOut Property


Description

Returns the PMaxOut result of the PNOP and PSAT marker search.

PMaxOut =  Marker 3 Y-axis value

 VB Syntax

pMaxOut = pMark.PMaxOut

Variable

(Type) - Description

pMaxOut

(double) - Variable to store returned value

pMark

A PNOP (object) or PSaturation (object)

Return Type

Double

Default

Not applicable

Examples

pMaxOut = pMark.PMaxOut 'Read

See example program

C++ Syntax

HRESULT get_PMaxOut(double* pNewVal)

Interface

IPNOP or IPSaturation