Read-only
About Diff I/Q App

ParameterList Property


Description

Returns a list of all existing parameters.

 VB Syntax

params = DIQ.ParameterList

Variable

(Type) - Description

params

(Variant Array) Comma-separated list of parameters, each parameter in the form  “name:expression”.

DIQ

A Differential I/Q (object)

Return Type

(Variant Array)

Default

Not Applicable

Example

params = diq.ParameterList 'Read

'Returns

"IPwrF1:a1_F1","OPwrF1:b2_F1","GainF1:b2_F1/a1_F1"

C++ Syntax

HRESULT get_ParameterList(VARIANT* params);

Interface

IDIQ