Differential I/Q is very flexible, allowing a variety of phase and frequency settings and measurements.
In this topic:
DIQ trace parameter example *.xml files are
stored on the PNA at:
C:\Users\Public\Documents\Network Analyzer\Samples\Setups\DiffIQ
Combines and extends the capabilities of ALL three of these features:
This allows you to set an internal or external source to any frequency range, any power level, and any phase relative to a defined reference source. Then, measure any receiver over any frequency range independent of the source frequency range(s), with optional match correction. Display the results of any receiver combination using mathematical expressions available with the Equation Editor feature.
The magnitude and phase of a controlled source is set relative to a reference source using a pair of receivers (one for the reference source and one for the controlled source), in an iterative loop. The controlled source is adjusted within the loop while measuring the ratio of the two receivers. The loop continues until either the desired magnitude and phase offset is achieved (within user-settable tolerance values), or the maximum number of iterations has occurred.
When controlling an external source, a portion of the output signal must be routed to an internal receiver (usually one of the reference receivers), via a splitter or directional coupler and one of the front- or rear-panel access points. The source can be controlled via any of the available remote interfaces, such as GPIB, USB, or LAN. The 10 MHz frequency reference should be shared between the source and network analyzer.
Frequency Offset Mode - Opt 080
Available ONLY on 4-port N522xA and N524xA (PNA-X) models.
The following Features are NOT Available in a Differential IQ channel:
Narrowband Pulse or Pulse Profile measurements using the Integrated Pulse App.
Define frequency ranges for sources and receivers.
Ranges can be fixed or swept frequency.
To accomplish necessary measurements, receivers can be tuned to an arbitrary list of frequencies independent of those used for the sources.
Define controlled sources for frequency, power, and phase relationships to other sources, using ranges from step 1.
Define trace parameters.
Parameters can use single receivers or multiple receivers combined with mathematical operators.
Parameters can combine receiver measurements made at different frequencies.
Define x-axis (can be frequency, power, phase, DC, points).
Calibrate all channels using the Cal All wizard, and if needed for additional direct-receiver response calibrations, the Cal Plan Manager wizard.
On the PNA front panel, press Meas, then [Measurement Class].
Select Differential I/Q, then either:
OK delete the existing measurement, or
New Channel to create the measurement in a new channel.
A Differential I/Q measurement is displayed.
Configure Differential I/Q settings |
|
Using
front-panel |
Using Menus |
|
|
Frequency Range (See Example configurations) Sets the source and receiver frequency range. Each defined frequency range can be measured by all of the PNA receivers. The Define Parameters dialog allows you to configure the measurements to be displayed. Only Linear sweeps are allowed. To make changes, click the Range Name to be changed, then click Edit to start the Frequency Range dialog. New - Creates a new frequency range. Remove - Deletes a range. This also removes all measurement parameters that use the deleted range. Sources Source Name - Lists the test ports through which an internal source is available. If an external source has been configured, it will appear at the bottom of the list. To make changes, click the Source Name to be changed, then click Edit to start the Source Configuration dialog. Add Source - Starts the External Source Configuration dialog.
|
|
To start this dialog, click the range name to be changed, then click Edit, in the above Differential IQ Setup dialog. Note: The Number of Points is always the same for ALL defined frequency ranges. Press Sweep, then Number of Points This dialog sets a frequency range for the source and receiver. The frequency range will be measured by ALL of the receivers. F1 can NOT be coupled to another range. IFBW - Set the IFBW to be used by the receivers for the specified frequency range. ProcedureEither set specific frequencies for the selected range:
Or set frequencies that are based on another already-created range:
How the selected range is calculatedFor the following frequency ranges (as seen in above dialog):
The following formula applies for each data point in each range: F3 = F1 * Multiplier / Divisor + F2 Note: The Number of Points is always the same for ALL defined frequency ranges. Press Sweep, then Number of Points ExamplesFor Mixers / Frequency Converters (See above dialogs)
For Amplifier Harmonics
|
|
This dialog is started by clicking the Source Name to be changed, then click Edit, in the Differential IQ Setup dialog. Configures the source for the specified port. You can set or sweep Power, Phase, and perform Match Correction for each source port. Source State: Choose from the following: Auto-on - Source power is turned ON at the specified test port when required by the measurement. This is the most common (default) setting. Auto-on sources are turned OFF when other sources are performing Match Correction sweeps. Always On - Source power is ALWAYS ON, regardless of measurements that are in process. Use this setting to supply source power to a DUT port that always requires power, such as an LO port. This could turn OFF power at another test port. Learn about internal second source restrictions. Off - Source power is turned off unless needed for match correction at a given port . Use this setting to prevent damage to a sensitive DUT test port. Uncontrolled - (External Sources ONLY). The source state and other settings are NOT changed. Match correction can NOT be performed while uncontrolled. PowerSweep Power - Check to perform a power sweep. Start / Stop Power - Set both the Start and Stop power levels for power sweep. Set a single (Start) power level for the specified source port. Leveling Mode: Choose from the following:
Source Attenuator: Enter source attenuation for the specified port number. Not available for external sources. Auto range source attenuator: Check to allow the analyzer to select the optimum attenuation value to achieve the specified test port power. Learn more. Power and Attenuators - Click to start the Power and Attenuators dialog. PhasePhase State - Choose from the following: Off - Phase is NOT set or controlled. Controlled - Phase is measured and iterated to within the specified tolerance. Specify the receivers and iteration properties to use to control phase. Open Loop - Phase and power is set, but receivers are NOT used to measure and iterate the phase or power of the source. Therefore, the setting of phase is not as accurate or stable. Open Loop mode can be used with phase sweep (for example, from 0 to 360 degrees). However, each sweep may not start at 0 degrees. NO settings on the Phase Control Setup dialog are used in Open Loop. Note: After selecting Open Loop, set each source to ON (not Auto) using the Power and Attenuators dialog. Sweep Phase Check to sweep on the specified source port. Start / Stop Phase - Set both the Start and Stop power levels for power sweep. Set a single (Start) power level for the specified source port Refer To - Select the port to which the controlled phase port is to be referenced. The two internal PNA sources are available ONLY at specific ports. These choices are limited for you. For example on a 4-port PNA-X, the possible port pairings are: 1/3, 1/4, 2/3, or 2/4. Port 1 can NOT be paired with Port 2, and Port 3 can NOT be paired with Port 4. Learn more about these limitations. Control Param. - Select the receivers to be used to measure the phase of the sources.
The swept phase or phase offset will be the difference between these two receivers. Only logical receiver notation (a1,b1) is available. Learn more. Select the receivers based on your application. You are responsible to make sure that your DUT configuration routes the signals of interest to the correct receivers. Otherwise, the phase will not be properly controlled. Phase Control Setup Click to launch the Phase Control Setup dialog. Note: When both Power and Phase are swept, both are swept SIMULTANEOUSLY in a single sweep. Match CorrectionMatch Correction On
Test Receiver - Select a test receiver to be used for Match Correction. Only logical receiver notation (b1, b2 and so forth) is available. Learn more. Reference Receiver - Select a test receiver to be used for Match Correction. Only logical receiver notation (a1, a2 and so forth) is available. Learn more. Select Frequency Range - Starts the following dialog. |
|
Match Correction Dialog help |
Select the frequency ranges over which Match Correction is to be performed. |
Four 'default' parameters are offered.
In addition, custom parameters can be defined using the Edit Parameters Dialog
How to select and configure Measurement Parameters |
|
Using front-panel
|
Using Menus |
|
|
Select one of the following 'default' parameters, or click Edit Parameters to show the following Edit Parameters dialog. Create in New Window - When checked, the selected measurements are created in a new window. |
|
ParametersSelect a predefined parameter from the list. Parameter Name - Change the 'default' name. Click Edit Name to start the virtual keyboard. Note: Do not use underscores in the parameter name. For example, b2_f1 cannot be used as a parameter name. However, b2f1 is a valid parameter name. To edit / create a parameter: Receiver - Select a receiver for which to plot measurement results. Frequency - Select the frequency range over which the results will be plotted. * (Operator) - Select an operator when combining multiple receivers. For example, when calculating differential or common mode parameters. ButtonsNew - Click to create a parameter. Remove - Click to delete the selected parameter. Save - Click to store the parameter to a *.diq file for later recall. Load - Click to recall a parameter that you previously defined and saved. The following are the contents from an example *.diq file that contains the above parameters. The file can be created using the above dialog, or edited directly using the format shown below.
|
||
How to Select X-Axis |
|
Using front-panel
|
Using Menus |
|
|
Select X-Axis Dialog help |
|||||||||||||
Select the domain to display on the X-axis of the window. Markers will be annotated and data files are saved using these choices. Choose from the following:
|
|||||||||||||
Calibration of the Differential IQ Channel is performed using the Cal All Calibration Wizard.
Cal All should be performed with all of the front panel jumpers in place and all of the path switches in the normal configuration. After the cal has been performed, the path switches can be set to the rear panel position if external sources are routed from the rear panel to the test ports.
This calibration appears as an S-parameter calibration in the Cal All Wizard.
When all four test ports are being used, but at least one port uses ONLY the source and its reference receiver, you can use the test port receiver for that port accessed through the front-panel jumper ports.
This measurement is calibrated by first performing the Cal All Calibration.
Then use the Cal Plane Manager - Direct Receiver Calibration to remove the effects of the transmission line that is used to connect the DUT to the receiver through the front-panel jumper port. See the detailed procedure.
Note: Only corrected scalar magnitude measurements are possible at the direct-access receiver. The phase information from the Cal All calibration is preserved in the Cal Set and is NOT modified by the Direct Access Receiver Cal.