Read-only
About Embedded LO

Parameter (Embedded LO) Property


Description

Returns the name of the parameter of the specified tuning sweep.

 VB Syntax

value = embedLODiag.Parameter (n)

Variable

(Type) - Description

value

(String) Variable to store the returned data.

embedLODiag

An EmbeddedLODiagnostic (object)

n

(Long) Tuning sweep number. Use NumberOfSweeps to find the number of sweeps taken.

Default

Not Applicable

Examples

data= embedLO.Parameter 3 'read

C++ Syntax

HRESULT Parameter(long sweep, BSTR * param);

Interface

IEmbededLODiagnostic