Write/Read
About PointAveraging

PointAveragingState Property


Description

Turns point averaging ON or OFF for all measurements on the channel.

 VB Syntax

chan.PointAveragingState = state

Variable

(Type) - Description

chan

A Channel (object)

state

(Enun)

False - Turns point averaging OFF

True - Turns point averaging ON

Return Type

Boolean

Default

False

Examples

chan.PointAveragingState = True 'Write

averg = chan.PointAveragingState 'Read

C++ Syntax

HRESULT get_PointAveragingState(BOOL *pVal)
HRESULT put_PointAveragingState(BOOL newVal)

Interface

IChannel16