Write/Read |
About Fixturing |
Description |
Sets and returns the Loss value at DC for the specified port number. Learn about Loss compensation values. Note: This command affects ALL measurements on the channel. |
VB Syntax |
fixture.PortLossDC(port) = value |
Variable |
(Type) - Description |
|
fixture |
A Fixturing (object) |
|
port |
(Integer) Port number to receive Loss value at DC. |
|
value |
(Double) Loss value in ohms. Choose a value between -90 and 90 |
Return Type |
Double |
Default |
0 |
Examples |
fixture.PortLossDC(2) = .002 'Write |
|
value = fixture.PortLossDC(1) 'Read |
|
C++ Syntax |
HRESULT get_PortLossDC(short port double *pVal) |
Interface |
IFixturing |