Read-only |
About Independent Power Calibration |
Description |
This property returns a handle to the PowerCalRange object. |
VB Syntax |
IndependentPwrrCal.PowerCalRange( ) |
Variable |
(Type) - Description |
IndependentPwrrCal |
A IndependentPowerCalibration (object) |
Return Type |
IPowerCalRange |
Default |
Not Applicable |
Example |
CalibrateAllChannels.IndependentPowerCalibration(3).PowerCalRange() |
C++ Syntax |
HRESULT PowerCalRange( IPowerCalRange** value); |
Interface |
IIndependentPowerCalibration |