Write/Read |
About Cal All |
Description |
Sets and returns the power offset value for a Cal All calibration. Power Offset provides a method of compensating port power for added attenuation or amplification in the source path. The result is that power at the specified port reflects the added components. |
VB Syntax |
calAll.PowerOffset (port) = value |
Variable |
(Type) - Description |
|
calAll |
A CalibrateAllChannels (object) |
|
port |
(Long) Source port number. |
|
value |
(Double) Power offset value in dB for a Cal All calibration.
|
Return Type |
Double |
Default |
0 (zero dB) |
Examples |
calAll.PowerOffset = 0 'Power Level of cal value = calAll.PowerOffset 'returns the power offset of the cal |
C++ Syntax |
HRESULT get_PowerOffset (long port, double val); HRESULT put_PowerOffset long port, double* newVal); |
Interface |
CalibrateAllChannels |
Last modified:
|
4-Jan-2012 |
New topic |