Write/Read |
About GainCompressionCalAbout SweptIMDCalAbout Guided Power Cal |
Description |
Set and read the cal kit to be used for calibrating at the adapter when the power sensor connector is different from the DUT. Use PowerSensorConnectorType to specify the connector type of the adapter. |
VB Syntax |
object.PowerSensorCalkitType = value |
Variable |
(Type) - Description |
object |
A GainCompressionCal (object) A SweptIMDCal (object) A GuidedCalibrationPowerSensor (object) |
value |
(String) - Cal Kit. Use CompatibleCalKits Property to return a list of valid cal kits. |
Return Type |
String |
Default |
Not Applicable |
Examples |
gca.PowerSensorCalkitType = "85052B" 'Write |
ctype = imd.PowerSensorCalkitType 'Read |
|
C++ Syntax |
HRESULT get_PowerSensorCalkitType(BSTR* Val) HRESULT put_PowerSensorCalkitType(BSTR newVal) |
Interface |
IGainCompressionCal2 ISweptIMD IGuidedCalibrationPowerSensor |
Last Modified:
8-Feb-2011 |
Added Guided |
9-Sep-2008 |
Added Swept IMD |
11-Apr-2008 |
MX New topic |