Write/Read |
About GainCompressionCalAbout SweptIMDCalAbout Guided Power Cal |
Description |
Set and read the power sensor connector type which is used to perform the Source Power Cal. Use PowerSensorCalKitType to specify the Cal Kit to use for the cal. |
VB Syntax |
object.PowerSensorConnectorType = value |
Variable |
(Type) - Description |
object. |
A GainCompressionCal (object) A SweptIMDCal (object) A GuidedCalibrationPowerSensor (object) |
value |
(String) - Power sensor connector type. Use ValidConnectorType Property to return a list of valid connector types. Select "Ignored" to NOT compensate for the adapter. |
Return Type |
String |
Default |
Not applicable |
Examples |
gca.PowerSensorConnectorType = "APC3.5 male" 'Write |
ctype = imd.PowerSensorConnectorType 'Read |
|
C++ Syntax |
HRESULT get_PowerSensorConnectorType(BSTR* Val) HRESULT put_PowerSensorConnectorType(BSTR newVal) |
Interface |
IGainCompressionCal2 ISweptIMDCal IGuidedPowerCalPowerSensor |
Last Modified:
8-Feb-2011 |
Added Guided |
9-Sep-2008 |
Added Swept IMD |
11-Apr-2008 |
MX New topic |