Write/Read |
About Guided Power CalAbout NFX Cal |
Description |
Set and read the power sensor connector type which is used to perform a Power Cal during an S-parameter calibration or during an NFX Cal. When used with Guided Power Cal, first enable a power cal using PerformPowerCalibration Property. |
VB Syntax |
guided.PowerSensorConnectorType (n) = value |
Variable |
(Type) - Description |
guided |
A GuidedCalibration (object ) |
n |
(Long) PNA port number to connect power sensor to. |
value |
(String) - Power sensor connector type. Use ValidConnectorType Property to return a list of valid connector types. Set to "Ignored" to NOT compensate for the adapter. |
Return Type |
String |
Default |
Not applicable. |
Examples |
guided.PowerSensorConnectorType(1) = "APC3.5 male" 'Write |
ctype = guided.PowerSensorConnectorType(1) 'Read |
|
C++ Syntax |
HRESULT get_PowerSensorConnectorType (long port, BSTR* val); HRESULT put_PowerSensorConnectorType (long port, BSTR newVal); |
Interface |
IGuidedCalibration6 |
Last Modified:
30-Nov-2010 |
Added index to example |
12-Oct-2009 |
MX New topic |