Write/Read |
About Power Sweep |
Description |
At the end of a power sweep, while waiting to trigger the next sweep, maintain source power at either the start power level or at the stop power level. |
VB Syntax |
pref.PowerSweepRetracePowerMode = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(Enum) - Choose from: 0 - naPowerSweepRetraceMode_Start - maintain source at start power level. 1 - naPowerSweepRetraceMode_Stop - maintain source at stop power level. |
Return Type |
Enum |
Default |
0 - naPowerSweepRetraceMode_Start |
Examples |
pref.PowerSweepRetracePowerMode = naPowerSweepRetraceMode_Start 'Write |
|
psMode = pref.PowerSweepRetracePowerMode 'Read |
|
C++ Syntax |
HRESULT get_PowerSweepRetracePowerMode (tagNAPowerSweepRetraceMode* preference); |
Interface |
IPreferences3 |
Last modified:
|
30-Aug-2010 |
Fixed Read example |
|
Oct. 25, 2006 |
New command |