Read only |
About PNA Options |
Description |
Returns the minimum specified frequency of the analyzer. Does not include any over-sweep. See also: MinimumFrequency Property |
VB Syntax |
value = cap.PresetMinFrequency |
Variable |
(Type) - Description |
|
value |
(Double) Variable to store the returned value. |
|
cap |
A Capabilities (object) |
Default |
Not Applicable |
Examples |
value = cap.PresetMinFrequency 'Read |
C++ Syntax |
HRESULT get_PresetMinFrequency(Double *value); |
Interface |
ICapabilities13 |