Write/Read
About Pulse Measurements

PulseProfileStart Property


Description

Sets and returns the start time of the pulse. Pulse profile measurements provide a time domain (CW frequency) view of the pulse envelope. Profiling is performed using a measurement technique that "walks" a narrow receiver "snapshot" across the width of the pulse. This is analogous to using a camera to take many small snapshots of a wide image, then piecing them together to form a single, panoramic view.

 VB Syntax

pulseMeas.PulseProfileStart = value

Variable

(Type) - Description

pulseMeas

A PulseMeasurementControl (object)

value

(double) - Start time in seconds.

Note: The start value cannot be negative.

Return Type

Double

Default

0

Examples

pulseMeas.PulseProfileStart = 3e-3 'Write

startprofile = pulseMeas.PulseProfileStart 'Read

C++ Syntax

HRESULT get_PulseProfileStart(double *pVal)
HRESULT put_PulseProfileStart(double pVal)

Interface

IPulseMeasControl3