Write/Read
About Diff I/Q App

RangeStartFrequency Property


Description

Sets and reads the start value for the specified frequency range.

On the Frequency Range dialog under Frequency, this is the Start setting.

 VB Syntax

DIQ.RangeStartFrequency (n)= value

Variable

(Type) - Description

DIQ

A Differential I/Q (object)

n

(Long) Frequency range number.

value

(Double)  Frequency range start value. Choose a value within the frequency range of the analyzer.

Return Type

Double

Default

Start frequency of the analyzer.

Examples

diq.RangeStartFrequency(2) = 1e9 'Write

value = diq.RangeStartFrequency(1) 'Read

C++ Syntax

HRESULT get_RangeStartFrequency(long range, double* RangeStartFrequency);

HRESULT put_RangeStartFrequency(long range, double RangeStartFrequency);

Interface

IDIQ