Write/Read
About Source Power Cal
About PMAR

ReferenceCalFactor Property


Description

Sets and returns the Cal Factor (%) for the 50 MHz reference signal associated with this power sensor. Use this property only if the power sensor does not contain cal factors in EPROM (for example, HP/Keysight 848x sensors).

 VB Syntax

pwrSensor.ReferenceCalFactor = value

Variable

(Type) - Description

pwrSensor

A PowerSensor (Object)

A PowerSensorAsReceiver (Object)

value

(double) – Cal factor in units of percent.  This can be any value between 1 and 150.

Return Type

Double

Default

100

Examples

pwrSensor.ReferenceCalFactor = 98 'R

RefFact = pwrSensor.ReferenceCalFactor 'Read

C++ Syntax

HRESULT put_ReferenceCalFactor(double newVal);

HRESULT get_ReferenceCalFactor(double *pVal);

Interface

IPowerSensor

IPowerSensorAsReceiver