Write/Read
About SA Application

SearchOccupiedBWMinFreq Property


Description

Set and read the minimum search frequency to use during an Occupied BW search measurement. Power below this frequency is ignored.

VB Syntax

sa.SearchOccupiedBWMinFreq = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Double) Minimum search frequency value.

Learn about these settings.

Return Type

Double

Default

250 MHz

Examples

sa.SearchOccupiedBWMinFreq = 300e6   Write

value = sa.SearchOccupiedBWMinFreq 'Read

C++ Syntax

HRESULT put_SearchOccupiedBWMinFreq(double minfreq);

HRESULT get_SearchOccupiedBWMinFreq(double* minfreq);

Interface

ISpectrumAnalyzer4