Write/Read |
About Security Level |
Description |
Controls the display of frequency information on the PNA screen and printouts. |
VB Syntax |
app.SecurityLevel value |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
value |
(enum NASecurityLevel) -Choose from: 0 - naNoSecurity ALL frequency information is displayed. 1 - naLowSecurity NO frequency information is displayed. Frequency information can be redisplayed using the Security Setting dialog box or this command. 2 - naHighSecurity LOW setting plus GPIB console is disabled. Frequency information can be redisplayed ONLY by performing a Preset, recalling an instrument state with None or Low security settings, or using this command. 3 - naExtraSecurity HIGH setting plus:
|
Return Type |
Long Integer |
Default |
0 - None |
Examples |
app.SecurityLevel = naLowSecurity 'Write |
|
level = app.SecurityLevel 'Read |
|
C++ Syntax |
HRESULT get_NASecurityLevel(tagNASecurityLevel *level); |
Interface |
IApplication4 |