Write/Read |
About Mixer/Converter Settings |
Description |
Set and read the fixed power level for the mixer segment. |
VB Syntax |
conv.SegmentFixedPower(index,range) = value |
Variable |
(Type) - Description |
|
conv |
|
|
index |
(Long integer) Segment for which power is being set. Choose a segment between 1 and the current segment count. Use SegmentCount Property to read the current count in the Applied Mixer. |
|
range |
(Enum as ConverterFrequencyRange) Range for which power is being set. Choose from: 0 - naInputFrequencies - set input power 1 - naOutputFrequencies - set output power 2 - naLO1Frequencies - set LO1 power 3 - naLO2Frequencies - set LO2 power 4 - naIFFrequencies - set IF power |
|
value |
(Double) Power level in dBm. Choose a value within the power/attenuation range of the PNA. |
Return Type |
Double |
Default |
|
Examples |
mxr.SegmentFixedPower(1,0)=0 'sets the input power level to 0 dBm |
C++ Syntax |
HRESULT get_SegmentFixedPower(long index, tagConverterFrequencyRange range, double *value); HRESULT put_SegmentFixedPower(long index, tagConverterFrequencyRange value, double value); |
Interface |
IConverter5 |
Last Modified:
|
26-Oct-2010 |
New command (A.09.33) |