Write/Read |
About Smoothing |
Description |
Specifies or returns the amount of smoothing as a ratio of the number of data points in the measurement trace. There is no COM command for specifying smoothing by number of aperture points. |
VB Syntax |
meas.SmoothingAperture = value |
Variable |
(Type) - Description |
|
meas |
A Measurement (object) |
|
value |
(double) - Smoothing Aperture. A ratio of (aperture points / trace points). Choose any number between .01 and .25. |
Return Type |
Double |
Default |
.25 |
Examples |
meas.SmoothingAperture = .10 'Write |
|
saperture = meas.SmoothingAperture 'Read |
|
C++ Syntax |
HRESULT get_SmoothingAperture(double *pVal) |
Interface |
IMeasurement |
Last modified:
|
Oct. 25, 2006 |
Fixed formula for smoothing |