Write/Read |
About SnP files |
Description |
Specifies the format of .SnP files. Use either app.Save (saves data to file) or meas.Get SnpDataWithSpecifiedPorts (reads data into variant array). |
VB Syntax |
pref.SnPFormat = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(string) - Format of the .S1P, .S2P, .S3P, .S4P data. Choose from: "MA" - Linear Magnitude / degrees "DB" - Log Mag / degrees "RI" - Real / Imaginary "Auto" - Format in which the trace is already displayed. If other than Log Mag, Linear Magnitude, or Real/Imag, then the format will be in Real/Imag. |
Return Type |
String |
Default |
"Auto" |
Examples |
pref.SnPFormat = "MA" 'Write |
|
format = pref.SnPFormat 'Read |
|
C++ Syntax |
HRESULT get_SnPFormat(BSTR *Format) |
Interface |
IPreferences |
Last Modified:
|
13-Jun-2011 |
Updated list to get method |