Read only |
About PNA Options |
Description |
Returns the string names of ports that can output a signal. The following is a list of string names for the PNA-X. Your PNA will NOT have all of these ports. Use GetPortNumber Method to return the correct port number for the specified port name.
For iTMSA (Opt 460)
This command also lists the External Sources that are currently configured and selected. To learn more, see Remotely Specifying a Source Port. |
VB Syntax |
value = object.SourcePortNames |
Variable |
(Type) - Description |
|
value |
(Variant array) - Variable to store the returned list of source port names. |
|
object |
A Channel (object) - always more complete than capabilities object. A Capabilities (object) - use when a channel is not available, or to find the common ports across all channels. |
Return Type |
Variant array of string names. |
Default |
Not Applicable |
Examples |
value = chan.SourcePortNames 'Read |
C++ Syntax |
HRESULT get_SourcePortNames(VARIANT *names); |
Interface |
IChannel13 ICapabilities4 |