Write/Read
About SA Application

SourcePowerPointCount Property

Description

Set and read the number of steps the source will make across the specified source power range. This setting is common to all sources.

VB Syntax

sa.SourcePowerPointCount = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Long)  Point count. Choose an integer value of 1 or higher.

Return Type

Long

Default

1

Examples

sa.SourcePowerPointCount = 10  'Write

value = sa.SourcePowerPointCount 'Read

C++ Syntax

HRESULT put_SourcePowerPointCount(long points);

HRESULT get_SourcePowerPointCount(long* points);

Interface

ISpectrumAnalyzer