Write/Read
About SA Application

SourcePowerRepeatCount Property

Description

Set and read the number of SA (receiver) sweeps for each Source Step. This setting is common to all sources.

VB Syntax

sa.SourcePowerRepeatCount = value

Variable

(Type) - Description

sa

A SpectrumAnalyzer (object)

value

(Long)  Repeat count. Choose an integer value of 1 or higher.

Return Type

Long

Default

1

Examples

sa.SourcePowerRepeatCount = 10   'Write

value = sa.SourcePowerRepeatCount 'Read

C++ Syntax

HRESULT put_SourcePowerRepeatCount(long count);

HRESULT get_SourcePowerRepeatCount(long* count);

Interface

ISpectrumAnalyzer