Write/Read
About NFX

SourcePullForSParameters  Property


Description

Enables and disables the use of source pull technique to compute S22 on Noise Figure on Converters. Learn more.

 VB Syntax

nfx.SourcePullForSParameters  = value

Variable

(Type) - Description

nfx

A NoiseFigure (object)

value

(Boolean)  Source pull technique state. Choose from:

False - Disable use of source pull technique.

True - Enable use of source pull technique.

Return Type

Boolean

Default

False

Examples

nfx.SourcePullForSParameters  = true 'Write

sourcePull = nfx.SourcePullForSParameters  'Read

C++ Syntax

HRESULT get_SourcePullForSParameters (VARIANT_BOOL * Val)

HRESULT put_SourcePullForSParameters (VARIANT_BOOL newVal)

Interface

INoiseFigure4