Write/Read |
About DC Sources |
Description |
Sets and returns Stop DC value for the specified DC source. |
VB Syntax |
dc.Stop (name,port) = value |
Variable |
(Type) - Description |
|
dc |
An DCStimulus (object) |
|
name,port |
(String) Name of the "DC source, port" Use Source Property to read a list of configured DC source names. To set the DC source to be always ON, do NOT specify a port. |
|
value |
(Double) DC Stop value. Choose a value within the range of the DC source. |
Return Type |
Double |
Default |
1 |
Examples |
'Set AO1 to always ON dc.Stop "AO1", 3 'Read Stop for MyDCSource,Port 1 dc.Stop? "MyDCSource,Port 1" |
C++ Syntax |
HRESULT get_Stop(BSTR name, VARIANT_BOOL * pValue); HRESULT put_Stop(BSTR name, VARIANT_BOOL newValue); |
Interface |
IDCStimulus |
Last Modified:
|
21-Feb-2012 |
MX New topic |