Write/Read |
About Ext DC Devices |
Description |
Sets and returns the "Dwell Before Sweep" value for an external DC Device which can be configured as either a DC Meter or a DC Source. |
VB Syntax |
extDC.SweepDwell = value |
Variable |
(Type) - Description |
|
extDC |
An ExternalDCDevice (object) |
|
value |
(Double) The dwell time (in seconds) before making a new sweep. |
Return Type |
Double |
Default |
1 milliseconds |
Examples |
extDC.SweepDwell = 10e-3 'Write |
|
dwell = extDC.SweepDwell 'Read |
|
C++ Syntax |
HRESULT get_SweepDwell (double *pValue) HRESULT put_SweepDwell (double newVal) |
Interface |
IExternalDCDevice |
Last Modified:
|
15-Feb-2012 |
New topic |