Read-only
About the ExtTestSetIO connector

SweepHoldOff Property


Description

Returns a boolean that represents the state of SweepHoldoff line (pin2) of the External Test Set connector.

 VB Syntax

value = ExtIO.SweepHoldOff

Variable

(Type) - Description

value

(boolean) - Variable to store the returned data

ExtIO

(object) - An External IO object

Return Type

Boolean

False  - indicates the line is being held at a TTL Low

True  - indicates the line is being held at a TTL High

Default

Not Applicable

Examples

value = ExtIO.SweepHoldOff

C++ Syntax

HRESULT get_SweepHoldOff(  VARIANT_BOOL* bValue);

Interface

IHWExternaTestSetIO