Write/Read
About IM Spectrum

SweepOrder Property


Description

Sets and returns the order number of IM products to view when SweepType = NTH  is specified. This actually sets the frequency span to DeltaF * N (this command value).

 VB Syntax

ims.SweepOrder = value

Variable

(Type) - Description

ims

An IMSpectrum Object

value

(Integer) Order number of IM product.

Return Type

Long Integer

Default

9

Examples

ims.SweepOrder = 5 'Write

value = ims.SweepOrder 'Read

C++ Syntax

HRESULT get_SweepOrder(long *pVal)
HRESULT put_SweepOrder(long newVal)

Interface

IIMSpectrum