Write/Read |
About Swept IMD |
Description |
Sets and returns the start power level of the Main tones. Use with IMD sweep type= naIMDTonePowerSweep. When tone power is coupled, setting either F1 or F2 power sets both. |
VB Syntax |
object.TonePowerStart (tone) = value |
Variable |
(Type) - Description |
|
object |
A SweptIMD or IMSpectrum Object |
|
tone |
(Enum as NAIMDTonePowerID) Choose from: 0 - naIMDF1Power - F1 tone 1 - naIMDF2Power - F2 tone |
|
value |
(Double) Start power in dBm. Choose a value between +30 dBm and -30 dBm. |
Return Type |
Double |
Default |
-20 dBm |
Examples |
imd.TonePowerStart(naIMDF1Power) = 0 'Write |
|
value = imd.TonePowerStart(naIMDF2Power) 'Read |
|
C++ Syntax |
HRESULT get_TonePowerStart(tagNAIMDTonePowerID naIMDF1, double * pVal); HRESULT put_TonePowerStart(tagNAIMDTonePowerID naIMDF1, double newVal); |
Interface |
ISweptIMD IIMSpectrum |