Write/Read
About PNA-X Touchscreen

Touchscreen Property


Description

Sets and reads the state of the PNA-X Touchscreen (ON and OFF).

This setting remains until changed again from the front-panel or remote command.

 VB Syntax

app.Touchscreen = state

Variable

(Type) - Description

app

An Application (object)

state

(boolean)

False (0) - Disables use of Touchscreen

True (1) - Enables use of Touchscreen

Return Type

Boolean

False - OFF

True - ON

Default

TRUE when shipped from factory.

Examples

app.Touchscreen = True 'Write

coupl = app.Touchscreen 'Read

C++ Syntax

HRESULT put_Touchscreen(VARIANT_BOOL bState)

HRESULT get_Touchscreen(VARIANT_BOOL *bState)

Interface

IApplication12