Click on image areas to learn more.
The PNA display is controlled by a third-party display driver. This driver is capable of producing many display effects which are beyond the basic needs of the PNA measurement environment. Keysight does not specify or warrant these display settings.
WARNING: The PNA display must remain in the 16 bit color setting in order to comply with international emissions regulations.
When using external programs to control the PNA, it is possible that the display settings may become corrupt. When this occurs, the following will restore the PNA display settings:
Click File then Minimize Application
Right-click on the desktop, then click Properties
On the Themes tab, select Keysight PNA
Click OK
The PNA is equipped with a 10.4-inch Hi resolution, color, touch-sensitive LCD screen for displaying traces, softkeys, and other measurement related information. The touch screen LCD allows you to make measurement settings by touching the LCD screen directly with a finger.
Learn more about the PNA-X Display area.
|
Important
|
How to Calibrate or turn ON | off the Touchscreen |
|
|
Using front-panel |
Using a mouse with PNA Menus |
|
|
|
|
|
|
The touchscreen ON |OFF setting remains until changed again from this menu, the Preferences dialog, or remotely. |
|
Provides details of each trace in the window. Highlighted trace indicates the active trace. Learn more.
The mouse-driven menu closely follows the menu structure of the front-panel hardkey/softkey menus. See Hardkeys to learn more about the logic of both menu structures.
Allows you to quickly undo and redo selected operations. Learn more
Along with the softkeys, allows numeric values to be entered for settings. Learn about all toolbars.
Provides stimulus and response information for markers. Learn about customizing the marker readout area. See also Marker Drag.
Provides window identification which is useful for remote programmers. only.
Provides detail about all aspects of the status of the analyzer. Learn more.
Displays the start and stop values of the sweep range.
Allows you to easily change the start and stop frequencies or start and stop power levels in a power sweep. Learn more.
See Also: Search Within
Drag a displayed marker across the trace using a finger (with touchscreen ON) or a mouse. Learn more.
Cursor changes to a “hand” when hovering over a clickable object.
Right-click on the Entry toolbar to launch a mouse-compatible numeric pad.
Windows
Right-click on a window area to make selections pertaining to that window.
Double-click on a window area to maximize the window. To return to original window configuration, right-click on window area, then click Tile.
Left-click on X-axis annotation to select the active channel/trace.
Right-click on X-axis annotation to change stimulus properties. Applications are not fully supported.
Quickly change Scale, Reference Level, and Position. Learn how.
Right-click on Y-axis annotation to change Scale.
Drag a trace from one window to another. Click or touch either the trace or the Trace Status. Drag the trace to another window, then release the mouse or lift your finger.
Left-click a trace or Trace Status to make it the selected trace.
Double-click on a trace or Trace Status to maximize the trace. Double-click again to return to the original trace configuration. See programming commands.
Set a preference to always widen the active trace.
Set a preference to briefly widen the active trace.
Drag a trace from one window to another. Click or touch either the trace or the Trace Status. Drag the trace to another window, then release the mouse or lift your finger.
Markers
Right-click on a trace or Trace Status to add a marker.
Right-click a marker to make selections pertaining to that marker, such as Marker Search or Function.
Click Utility, then System, then Keys toolbar to show and hide the simulated hardkeys.
The combination of hard keys and softkeys allow easy access to ALL analyzer features.
One additional softkey is reserved as a User Key which is always visible. Learn more.
To Hide the softkeys to make more room for measurement windows, right-click any softkey.
To Show the softkeys, press any front-panel hardkey that launches a softkey menu.
The Hide/Show choice is reset to the default (Show) only on analyzer startup (NOT on Preset).
Softkey Annotations
|
Item |
Description |
|
|
Selection launches a dialog box. |
|
|
Selection launches another level of softkeys. |
|
|
Indicates the item (marker, trace, window) is ON. Any number of objects can be ON. |
|
|
Indicates the item (marker, trace, window) is OFF. Click to turn item ON. |
|
|
Indicates the item IS selected. |
|
|
Indicates the item is NOT selected. Click to select. Only one item in the collection can be ON. |
|
|
Enter value in Entry toolbar. |
|
|
Capitalization indicates the current setting. |
|
|
Return to the previous softkeys. |
|
|
Launches more of the same level softkeys. |
Choose from several popular menus to assign to the User key. Menu structures for existing and future applications can also be selected as the User Key. The most flexible of the User Key selections is Favorites.
How to setup the User Key |
|
|
Using front-panel |
Using Menus |
|
|
|
Assigns the selected function to the User (soft) Key on the main display. The User Key is always visible on the display. Blank Leave the User Key Blank - no assignment. Allows you to select and display any eight softkeys from any level. Your Favorite menu selections are always two button presses away. Note: Applications softkeys that are created as Favorites do NOT survive a Preset.
Setup Measurement When assigned to the User Key, press the Setup Measurement softkey to populate the softkeys with measurement settings that are relevant for the active trace. For example, when a Gain Compression measurement is active, press Setup Measurement to quickly access the GCA setup dialog. Marker Functions, Transform, Gating When any of these functions are assigned to the User Key, one press of the User Key and the softkeys are populated with the most common settings for the corresponding function. Undo Quickly access the Undo/Redo feature. Learn more. |