Write/Read
About IM Spectrum

TrackingChannel Property


Description

Sets and returns the IMD channel number to which the IM Spectrum channel is coupled. Use TrackingEnable to enable tracking.

 VB Syntax

ims.TrackingChannel = value

Variable

(Type) - Description

ims

An IMSpectrum Object

value

(Integer) Existing IMD channel number to which frequency and power settings are coupled.

Return Type

Long Integer

Default

First existing IMD channel

Examples

ims.TrackingChannel = 1 'Write

value = ims.TrackingChannel 'Read

C++ Syntax

HRESULT get_TrackingChannel(long *pVal)
HRESULT put_TrackingChannel(long newVal)

Interface

IIMSpectrum