Write/Read
About IM Spectrum

TrackingEnable Property


Description

When an IMD channel exists, allows the IM Spectrum frequency and power setting to track (couple with) the IMD channel settings. Use TrackingChannel to set the channel number to track.

 VB Syntax

ims.TrackingEnable = value

Variable

(Type) - Description

ims

An IMSpectrum Object

value

(Boolean) Tracking state. Choose from:

True - IM Spectrum frequency and power settings track the IMD channel settings.

False - IM Spectrum frequency and power settings are specified in the IMS channel.

Return Type

Boolean

Default

False

Examples

ims.TrackingEnable = True 'Write

value = ims.TrackingEnable 'Read

C++ Syntax

HRESULT get_TrackingEnable(VARIANT_BOOL* bValue)
HRESULT put_TrackingEnable(VARIANT_BOOL newVal)

Interface

IIMSpectrum