Write/Read
About Marker Search

Tracking Property


Description

This property, when on, executes the search function (marker.SearchFunction) every sweep.

In effect, turning Tracking ON is the same as executing one of the immediate, one-time, "Search..." methods (such as SearchMin, SearchMax) for every sweep.

 VB Syntax

mark.Tracking = state

Variable

(Type) - Description

mark

A Marker (object)

state

(boolean) - Tracking state. Choose from:

False - Tracking OFF

True - Tracking ON

Return Type

Boolean

Default

False

Examples

mark.Tracking = False 'Write

markTracking = mark.Type 'Read

C++ Syntax

HRESULT put_Tracking(VARIANT_BOOL bOn)
HRESULT get_Tracking(VARIANT_BOOL * pbOn)

Interface

IMarker