Write/Read
About Trigger

TriggerDelay Property


Description

Sets and reads the trigger delay for all measurements (GLOBAL). This delay is only applied while in app.Source = naTriggerSourceExternal and trigsetup.Scope = naGlobalTrigger .  After an external trigger is applied, the start of the sweep is delayed for the specified delay value plus any inherent latency.

To apply a trigger delay for a channel only, use ExternalTriggerDelay Property.

 VB Syntax

app.TriggerDelay = value

Variable

(Type) - Description

app

An Application (object)

value

Double- Trigger delay value in seconds. Range is from 0 to 3.

Return Type

Double

Default

0

Examples

app.TriggerDelay = .003  'Write

delay = app.TriggerDelay 'Read

C++ Syntax

HRESULT get_TriggerDelay(double *delay);

HRESULT put_TriggerDelay(double delay)

Interface

IApplication