Write/Read. |
About Trigger |
Description |
Note: This property has been replaced with Scope Property. Sets or returns the trigger type which determines the scope of a trigger signal. |
VB Syntax |
app.TriggerType = value |
Variable |
(Type) - Description |
app |
An Application (object) |
value |
(enum NATriggerType) - Trigger type. Choose from: 1 - naChannelTrigger - a trigger signal is applied to the current channel. The next trigger signal will be applied to the next channel; not necessarily channel 1-2-3-4. |
Return Type |
Long Integer |
Default |
naGlobalTrigger |
Examples |
app.TriggerType = naGlobalTrigger 'Write |
trigtyp = app.TriggerType 'Read |
|
C++ Syntax |
HRESULT get_TriggerType(tagNATriggerType *pTrigger) |
Interface |
IApplication |