Read/Write
About Embedded LO

TuningMode Property


Description

Sets and returns the method used to determine the embedded LO Frequency.

 VB Syntax

obj.TuningMode = value

Variable

(Type) - Description

obj

An EmbeddedLO (object) or

A ConverterEmbeddedLO (object)

value

(Enum as NAEmbeddedLOTuningMode)

Tuning mode. Choose from:

0 - naEmbeddedLOTuningMode_Broadband_And_Precise

1 - naEmbeddedLOTuningMode_Precise_Only

2 - naEmbeddedLOTuningMode_None

Return Type

(Enum)

Default

0 - naEmbeddedLOTuningMode_Broadband_And_Precise

Examples

embedLO.TuningMode = naEmbeddedLOTuningMode_None 'write

value = embedLO.TuningMode 'read

C++ Syntax

HRESULT get_TuningMode(enum NAEmbeddedLOTuningMode* mode);

HRESULT put_TuningMode(enum NAEmbeddedLOTuningMode mode);

Interface

IEmbededLO