Write/Read | 
About Marker Types | 
Description | 
 Sets and reads the marker type.  | 
VB Syntax | 
 mark.Type = value  | 
Variable | 
(Type) - Description | 
| 
 chan  | 
 A Marker (object)  | 
| 
 value  | 
 (enum NAMarkerType) - Marker Type. Choose from: 1 - naMarkerType_Fixed - retains and keeps its x-axis value at the time the marker type is set.  | 
Return Type | 
 Long Integer  | 
Default | 
 naMarkerType_Normal  | 
Examples | 
 mark.Type = naMarkerType_Normal 'Write  | 
| 
 MrkType = mark.Type 'Read  | 
|
C++ Syntax | 
 HRESULT get_Type(tagNAMarkerType *pVal)  | 
Interface | 
 IMarker  |