Write/Read |
About Limits |
Description |
Specifies the Limit Line type. |
VB Syntax |
limt(index).Type = value |
Variable |
(Type) - Description |
limt |
A LimitSegment (object) |
index |
(variant) - Limit line number in the LimitTest collection |
value |
(enum NALimitSegmentType) - Limit Line type. Choose from: |
Return Type |
Long Integer |
Default |
0 - OFF |
Examples |
Set limts = meas.LimitTest |
limitType = limts.Type 'Read |
|
C++ Syntax |
HRESULT put_Type(tagNALimitSegmentType *pVal) |
Interface |
ILimitSegment |