Write/Read |
About Phase Reference Cals |
Description |
Sets and returns the LO Frequency to the unknown mixer. |
VB Syntax |
phaseRef.UnknownMixerLOFrequency = value |
Variable |
(Type) - Description |
|
object |
PhaseReferenceCalibration (object) |
|
value |
(Double) LO frequency in Hz. Choose a value between 3 GHz and (Max Frequency minus 1GHz). For a 26.5 GHz PNA, the range is 3 GHz to 25.5 GHz. For best results, use the default LO frequency. 3.351Ghz. This frequency produces no spurs from the input/LO frequency. And also the Input frequency will have no band breaks. |
Return Type |
Double |
Default |
3.351 GHz |
Examples |
phaseRef.UnknownMixerLOFrequency = 3.351e9 |
|
value = phaseRef.UnknownMixerLOFrequency 'Read |
|
C++ Syntax |
HRESULT get_UnknownMixerLOFrequency(double *value) HRESULT put_UnknownMixerLOFrequency(double value) |
Interface |
IPhaseReference2 |
Last Modified:
|
15-Mar-2013 |
New topic |