Write/Read |
About User Ranges |
Description |
Note: This property on the Channel Object is superseded by the same property on the Measurement Object. Sets the stimulus stop value for the specified User Range. |
VB Syntax |
chan.UserRangeMax(domainType,Rnum) = value - Superseded meas.UserRangeMax(Rnum) = value mark.UserRangeMax(Rnum) = value |
Variable |
(Type) - Description |
|
chan |
A Channel (object) - Superseded |
|
meas |
A Measurement (object) |
|
mark |
A Marker (object) To assign a marker to a User Range, use the UserRange Property. |
|
domainType |
This argument is no longer required. The domain type is inferred by the measurement or marker. (enum NADomainType) - Choose from: 0 - naDomainFrequency 1 - naDomainTime 2 - naDomainPower |
|
Rnum |
(long integer) - User Range number. Choose any number between 1 and 16 (0=Full Span) |
|
value |
(double) - Stop value. Choose any number within the full span of the channel. |
Return Type |
Double |
Default |
The current stimulus setting for the channel |
Examples |
mark.UserRangeMax(1) = 3e9 'Write meas.UserRangeMax(1) = 3e9 'Write |
|
UseRngeMax = mark.UserRangeMax(1) 'Read UseRngeMax = meas.UserRangeMax(2) 'Read |
|
C++ Syntax |
HRESULT put_UserRangeMax(long rangeNumber, double maxValue) HRESULT get_UserRangeMax(long rangeNumber, double *maxValue) |
Interface |
IMeasurement IMarker |
Last Modified:
|
3-May-2011 |
Updated for measurement object |