Write/Read |
About User Ranges |
Description |
Sets the stimulus start value for the specified User Range. This property uses different arguments for the channel and marker objects. |
VB Syntax |
chan.UserRangeMin(domainType,range) = value or mark.UserRangeMin(range) = value |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
mark |
A Marker (object) To assign a marker to a User Range, use the UserRange Property. |
|
domainType |
Note: The Marker object does not require the domainType argument. (enum NADomainType) Type of sweep currently implemented on the channel - Choose from: 0 - naDomainFrequency 1 - naDomainTime 2 - naDomainPower 3 - naDomainPhase |
|
range |
(long) - User Range number. Choose any number between 1 and 16 (0=Full Span) |
|
value |
(double) - Start value. Choose any number within the full span of the analyzer |
Return Type |
Double |
Default |
The current stimulus setting for the channel |
Examples |
mark.UserRangeMin(1) = 3e9 'Write |
|
UseRngeMin = mark.UserRangeMin 'Read |
|
C++ Syntax |
HRESULT put_UserRangeMin(tagNADomainType domain, long rangeNumber, double minValue) |
Interface |
IChannel |
Last Modified:
|
3-May-2011 |
Updated for phase |