Write/Read
About Vector Averaging

VectorAverageEnable Property


Description

Set and read the ON/OFF state of the vector averaging.

VB Syntax

sa.coherence.VectorAverageEnable = value

Variable

(Type) - Description

sa.coherence

A SpectrumAnalyzerCoherence (object)

value

(Boolean) Choose from:

0 - OFF - Vector averaging is set to OFF.

1 - ON - Vector averaging is set to ON.

Learn about these settings.

Return Type

Boolean

Default

0

Examples

sa.coherence.VectorAverageEnable = OFF   Write

value = sa.coherence.VectorAverageEnable 'Read

C++ Syntax

HRESULT put_VectorAverageEnable(VARIANT_BOOL bEnable);

HRESULT get_VectorAverageEnable(VARIANT_BOOL* bEnable);

Interface

ICoherenceSA