Write/Read
About X-Axis Spacing

XAxisPointSpacing Property


Description

Sets X-axis Point Spacing for the displaytraces measured with segment sweeps on the active channel.

 VB Syntax

chan.XAxisPointSpacing = value

Variable

(Type) - Description

chan

A Channel (object)

value

(Enum as naStates) - Choose from:

0 - naOFF - Turns X-axis Point Spacing OFF

1 - naON - Turns X-axis Point Spacing ON

Return Type

Enum

Default

0 - naOFF

Examples

chan.XAxisPointSpacing = naOFF 'Write

xspac = chan.XAxisPointSpacing 'Read

C++ Syntax

HRESULT get_XAxisPointSpacing (tagNAStates *pState);
HRESULT put_XAxisPointSpacing (tagNAStates newState);

Interface

IChannel2